The packaging technology expert RemiTech specialises in material transport systems such as belt conveyors, roller conveyors and turntables. The company also covers process automation, such as product sorters or positioners in packaging lines.
For a customer in the food supplement sector, a packaging line was to be created that automatically packs containers with the food supplement. A pick-and-place robot was to be used to load the containers with portioning spoons, which would work independently and continuously at the end of the packaging line.
Due to the hygiene standards and the fine powder particles in the product containers and in the immediate vicinity, no metallic solutions could be used as spherical bearings on the axes of the delta robot. As the bearings have to be lubricated externally, grease could leak out and contaminate the product. At the same time, particles could adhere to the lubricant and limit the service life of the bearing technology.
Instead, a completely dirt-proof and dust-resistant solution had to be found. This primarily concerns the spherical bearings, which are intended to ensure the smooth movement of the delta robot's axes.