Change Language :
The igus Robot Control software enables simple and intuitive robot programming and control systems, making it easy to get started with automation. Thanks to the modular structure, various robot kinematics, e.g. delta robots, linear robots and multi-axis articulated robots can be controlled. The software can be used to simulate the individual movements of the robot on the 3D surface – the robot does not need to be connected for this step.
Programming examples of various applications with the robot software
System requirements:
The PLC interface (PLC = Programmable Logic Controller) enables the execution of basic functions and the signalling of states by means of digital inputs and outputs. In addition to the control by a PLC, this interface also enables operation via hardware buttons.
Robot programs can be loaded and started and gripper commands can be sent via digital inputs or global signals. This is useful, for example, if a program is to be selected from a given selection using buttons or the CRI-GSig instruction.
The Modbus TCP interface can be used to send PLC data and instructions to the robot control system and receive status information, for example.
The CRI interface enables complex instructions to be sent and information and settings to be retrieved via the Ethernet interface using TCP/IP. The igus Robot Control uses this interface to connect to robots with an integrated control system or other instances of the control system.
The camera interface enables the use of object detection and video cameras. Object detection cameras recognise the position and class of objects and transmit these, optionally with a video image, to the control system. The control system calculates positions in the robot coordinate system from the object positions of the camera. Pure video cameras only deliver images and can therefore only be used to monitor the work area, but not to detect objects.
The Cloud interface enables the robot to be monitored via RobotDimension. Once activated and logged in, the robot sends basic status information and camera images to the online service. The user can list their robots on the website and retrieve the information.
Integrate the robots into your ROS environment. Documentation and packages for hardware communication, Teleop and moveI

The assembled tool can be specified here. Changing the tool requires the project to be reloaded or the integrated control system to be restarted. New tools can be defined as a configuration file in the directory "Data/Tools"

The range of movement of the robot arm is restricted by the settings of the virtual box. This functionality helps to prevent mechanical damage and simplifies programming, depending on the application. If a program is executed that violates the virtual box, it is stopped with an error message.

The robot control system supports up to 3 additional axes (also called "external axis" in iRC). These can be installed according to the robot axes and configured via the configuration area of iRC.

Here you can define the robot and logic program, the movement speed (as a percentage of the maximum speed), the playback mode and the reaction to program errors.

The robot control system can be customised for your robot with a digital twin. We configure the inverse kinematics to suit your project business.

The Joint command moves the robot to an absolute target position that is specified in axis coordinates (e.g. axis angle or position of a linear axis). The resulting movement of the TCP is usually a curve and not a straight line.

The Linear command moves the robot to an absolute target position specified in Cartesian coordinates. The resulting movement of the TCP follows a straight line.

The instruction "Circular movement" enables movements along a full or partial circular path. It is compatible with linear movements so that the transition from and to linear movements can be smoothed over.

Conditions can be used in if-then-else commands, loops and as cancellation conditions in motion commands. The conditions can be combinations of digital inputs, global signals, Boolean operations and comparisons.

The grid instructions calculate positions aligned to a grid, e.g. as a gripping or depositing position for palletising tasks.

The Relative command allows you to move the robot relative to its current position. It can be accessed via the menu items under "Action" → "Relative movement".

Sub-programs can be called up with the sub-command. The path to the sub-program file is specified under "File name". It is relative to the subfolder "Programs" of the iRC folder "Data".

Two types of variables are supported in the program for igus Robot Control and TinyCtrl:

The licence-free igus Robot Control software is integrated into the control system and therefore uses a standardised operating concept and consistent communication services for many components of one system. This means less project planning work and faster commissioning.
In person:
Monday to Friday from 7 am - 8 pm.
Saturdays from 8 am- 12 pm.
Online:
24h
WhatsApp-Service:
Montag – Freitag: 8 – 16 Uhr