Configurators for triflex® R energy chain

Quick Robot

The configurator for the complete robotic system

The configurator offers the possibility to design a complete energy supply package from axis 2 to axis 6. Possible for the following manufacturers: 
  • ABB
  • Fanuc
  • Kuka
  • Yaskawa
  • Universal Robots
  • Techman Robot
Start the configurator

Augmented reality feature in Quick Robot

AR in the update

Update for HMI 2023

We are constantly trying to improve good things like the Quick Robot and have added a new feature to the tool for the Hannover Messe 2023.
For three robot models, each with a specific configuration, we offer the option of representing an ABB, Fanuc and Kuka robot as an augmented version. 
Experience the visualisation of your project in a whole new dimension.   
Test the AR update

Add cables & hoses directly in the configurator

With the online tool, you can quickly and easily configure the right system for the respective robot.
But the size of the respective system must also be adapted to the cables and hoses (filling). Ideally, the filling level of the e-chain® should not exceed 60%. 
To ensure that the correct size of system is selected, the filling can be integrated directly in the online tool.     

Interior separation for all triflex R series

When choosing the right triflex R size, make sure that a clearance space is planned for all electrical, pneumatic and media cables. This is necessary to compensate for forces that occur due to relative movements between the e-chain® and the cables as well as between the cables themselves. Cables must be installed with sufficient clearance. The following value can be assumed as a rough rule of thumb: the sum of the cable cross sections should not exceed 60% of the effective cross section; in addition, a space requirement of 10% or at least 1mm to the next cable or e-chain® must be observed. The quickest and easiest solution to find the correct triflex R filling is the interior separation configurator, where all triflex R series are available
Start the configurator

Maximum filling 

Well-filled triflex R

Consulting

I look forward to answering your questions

Shipping and consultation

In person:

Monday to Friday from 7 am - 8 pm.
Saturdays from 8 am- 12 pm.

Online:

24h


The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "igutex", "kineKIT", "manus", "motion plastics", "pikchain", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention on this website. The products offered by igus® are those of igus® GmbH