My contact person
e-chains®, chainflex®, cables, harnessed systems readychain®

27113121848
Photo
dry-tech® bearing technology

27113121848
Photo

Interactive exhibits for a distillery visitor centre

A series of interactive exhibits were designed and developed for a distillery visitor centre in Scotland using igus®’ iglidur® slewing rings. The interactive exhibits consisted of a series of submarine style periscopes operated by the visitor to gain a 360 degree view of the exterior landscape. An additional periscope was designed and built for handicapped access. A way had to be found of making the periscopes sit on their respective poles and turn freely, which a normal bearing would allow, but also stop them from turning so freely as to allow the public to spin them. A solution was needed which didn't include a brake which would wear over time. This became achievable without introducing a separate braking component. The iglidur® polymer based PRT slewing rings allowed for low friction rotation and offered a degree of rotational resistance. Additionally, they offered lightweight and maintenance free properties.

Stephen Sheffield
Project Manager
The Glue Factory

More on applied products here

More interesting applications from diverse areas can be found here